How can we help you today?

Is It possible to mix standard powered sensors and two-wire sensors on the 4-5-6 inputs of the STBACI1400 module?

You cannot mix standard powered sensors and two-wire sensors on the 4-5-6 inputs of the STBACI1400 because input 6 serves as the "return" or common for inputs 4 and 5.

For powered sensors, connect input 3 or 6 to the sensor, not to the (-) of the power supply.

EXAMPLE:

For Powered sensors:

Wiring diagram 1

For 2 wires sensors:

Wiring diagram 2

Best Regards.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center