How can we help you today?

I have a Windows Industrial PC (iPC), which Vijeo Designer Runtime License do I need?

Issue

I have a Windows iPC, which Vijeo Designer Runtime License do I need? This FAQ goes through the different types of Schneider Electric branded and unbranded Industrial PCs and provides the required Vijeo Designer Runtime License part number.

Product Line

Vijeo Designer Runtime

Environment

Windows-based Industrial PC (iPC) - Schneider Electric branded or non-branded

Resolution

There are 6 main part numbers for Vijeo Designer Runtime single seat (one license per device) licenses for Windows-based Industrial PCs (iPCs):

VJDRTPROH1P - Vijeo Designer v6.3 Runtime License for Harmony P6 / PSA6

VJDRTPROS1P - Vijeo Designer v6.3 Runtime License for (a) Standard iPCs, (b) Legacy Harmony/Magelis iPCs, (c) Generic Standard PCs, or (d) Third-party iPCs

VJDHPCCZLSPAZZ - Vijeo Designer v6.2 (SP11 and SP12) Runtime License for Harmony families: HMIBMP, HMIBMU, HMIPSO, HMIPSP, HMIPEP, P6

VJDRPCCZLSPAZZ - Vijeo Designer v6.2 (SP11 and SP12) Runtime License for Standard PC and Harmony HMIBMI/HMIBMO (excluding families: HMIBMP, HMIBMU, HMIPSO, HMIPSP, HMIPEP)

VJDSNRTSPC - Vijeo Designer Runtime License for v6.2.10 SP10 or lower for Schneider Electric branded iPCs

VJDSNRTMPC - Vijeo Designer Runtime License for v6.2.10 SP10 or lower for Generic Standard PCs, or Third-party iPCs

For more details see the tables below.

For currently offered Schneider Electric branded Industrial PCs (as of 2026 Q3):

iPC ModelSingle Seat Runtime License Part Number for Specified Version of Vijeo Designer
v6.2.10 (SP10) or olderv6.2.11 (SP11) to v6.2.12 (SP12)v6.3.x
Harmony P6 /  P6 Basic Box (Modular Box PCs)VJDSNRTSPCVJDHPCCZLSPAZZVJDRTPROH1P
Harmony PSA6 (All-in-one Panel PCs)VJDSNRTSPCVJDHPCCZLSPAZZVJDRTPROH1P
Harmony HMIG5U22<license not required><license not required><license not required>
Harmony HMIG5U21<license not required><license not required><license not required>

NOTE: For HMIG5U21 hardware, choose model "HMIG5U" in Vijeo Designer Buildtime.

Previously Offered iPCs from Schneider Electric that are no longer produced:

iPC ModelSingle Seat Runtime License Part Number for Specified Version of Vijeo Designer
v6.2.10 (SP10) or olderv6.2.11 (SP11) to v6.2.12 (SP12)v6.3.x
BOX Performance HMIBP***2/HMIBP***5VJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
BOX Universal HMIBU***1/HMIBU***2VJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Enclosed PC Performance HMIPEP*9VJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Magelis Box Performance HMIBMPVJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Magelis Box Universal HMIBMUVJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Panel Performance HMIPP*6 / HMIPP*7 / HMIPR*7 / HMIPP*9VJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Panel Universal HMIPU*6 / HMIPU*7 / HMIPU*9VJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Rack PC Optimized HMIRSO / HMIRXOVJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Rack PC Performance HMIRSPVJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Rack PC Universal HMIRSUVJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
S-Panel Optimized HMIPSO*5 / HMIPSO*7VJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
S-Panel Performance HMIPSP*7 / HMIPSP*9VJDSNRTMPCVJDHPCCZLSPAZZVJDRTPROS1P
Harmony HMIG5U2<license not required><license not required><license not required>
Magelis HMIG5U<license not required><license not required><license not required>
Magelis HMIBMI Edge BoxVJDSNRTSPCVJDRPCCZLSPAZZVJDRTPROS1P
Magelis HMIBMO Edge BoxVJDSNRTSPCVJDRPCCZLSPAZZVJDRTPROS1P

Other iPCs:

iPC ModelSingle Seat Runtime License Part Number for Specified Version of Vijeo Designer
v6.2.10 (SP10) or olderv6.2.11 (SP11) to 6.2.12 (SP12)v6.3.x
Any Schneider Electric Windows-Based iPC not listed in above tablesVJDSNRTSPCVJDRPCCZLSPAZZVJDRTPROS1P
Any Third-Party Windows-based Industrial PCVJDSNRTSPCVJDRPCCZLSPAZZVJDRTPROS1P
Any Windows laptop or personal computerVJDSNRTSPCVJDRPCCZLSPAZZVJDRTPROS1P

For all other Vijeo Designer licenses or multi-seat licenses, see the Vijeo Designer- Classic HMI Configuration software Catalog (document reference DIA5ED2130614EN):

https://www.se.com/us/en/download/document/DIA5ED2130614EN/

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center