How can we help you today?

How to view the complete details and information of an APC Back UPS_(BR, BN and BK Series) using the Power Chute interface.

Issue:  How to view the complete details and information of an APC Back UPS_(BR, BN and BK Series) using the Power Chute interface.


Product Line: BR900G2-FR, BR900G2-GR, BR900G2I, BR650G2I, BK650G2I, BK500G2I, BK350G2, BN1050M2, BX1000M2, BX850M2, BR700G2, and BK500G2.

Resolution:  UPS models BR900G2-FR, BR900G2-GR, BR900G2I, BR650G2I, BK650G2I, BK500G2I, BK350G2, BN1050M2, BX1000M2, BX850M2, BR700G2, and BK500G2 is capable of connecting to PCSS (Power Chute Serial Shutdown) because it has a Data port. Through PCSS there is an option for the following UPS models to view the complete details of a UPS.



See simple instructions below:

1. From the PCSS interface, go to "ABOUT"

See screenshot below:

details 1

2. Click "About": see screenshot below:

details 2

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center