How can we help you today?

Manual Cleanup After Unsuccessful Installation or Uninstallation of PowerChute Network Advanced

Issue

This article describes the manual procedure for removing PowerChute Network Advanced after an unsuccessful installation or uninstallation.

Products

PowerChute Network Advanced Configuration Tool version 1.0

Environment

Windows

Solution

Use this procedure if installation or uninstallation is unsuccessful and leaves a partial PowerChute Network Advanced setup behind:

1. Log in to the computer where PowerChute Network Advanced is installed with a local administrator account.
2. Close the PowerChute Network Advanced user interface and any open installer windows.
3. Open Services and stop the PowerChute service if it is still running.
4. If the service cannot be stopped in Services, open an elevated Command Prompt and run:

sc stop PCNA
sc delete PCNA

Delete Registry Entries (RegEdit)
Open Registry Editor as administrator and remove the following keys if they exist:

1. HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\PowerChute Network Advanced
2. HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\PowerChute Network Advanced
3. HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Services\PCNA

Important:

  • Delete only the keys listed above.
  • If a key is missing, continue with the next one.

Delete Shortcuts

1. Start Menu shortcut:
- Go to C:\ProgramData\Microsoft\Windows\Start Menu\Programs
- Delete the Schneider Electric folder or the PowerChute Network Advanced shortcut, if present.

2. Desktop shortcuts:
- All users' desktop: C:\Users\Public\Desktop
- Current user desktop: C:\Users\<username>\Desktop
- Delete any PowerChute Network Advanced shortcut files found.

Delete Installation Folder

1. Delete C:\Program Files\Schneider Electric\PowerChute Network Advanced
2. If the C:\Program Files\Schneider Electric folder is empty after that, it can also be deleted.

Final Verification

1. Confirm the PCNA Windows service is no longer present in Services.
2. Confirm the three registry keys listed above are removed.
3. Confirm no PowerChute shortcuts remain in the Start Menu or on the Desktop.
4. Reboot the machine before retrying installation.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center