PowerChute Network Advanced - Session Timeout Configuration
Issue
This article describes how to configure the session timeout for the PowerChute Network Advanced Configuration Tool. The session timeout determines how long a user session remains active before the user is automatically logged out due to inactivity.
Products
PowerChute Network Advanced Configuration Tool version 1.0
Environment
Windows
Solution
Requirements
- Permission to edit configuration files in the PowerChute Network Advanced installation directory
- Permission to restart Windows services
Configuration Steps
Step 1: Locate the Configuration File
Navigate to the `config` folder in your PowerChute Network Advanced installation directory and open the `application.properties` file in a text editor.
Step 2: Find the Session Timeout Property
Locate the following line in the configuration file:
# Session inactivity timeout (e.g. 15m, 1h) # You can use the following suffixes: ms (milliseconds), s (seconds), m (minutes), h (hours), d (days). # Note: A number without a suffix is treated as milliseconds. server.servlet.session.timeout=15m
Step 3: Modify the Timeout Value
Change the session timeout value to your desired duration. For example:
| Session Timeout | Configuration |
|---|---|
| 30 minutes | `server.servlet.session.timeout=30m` |
| 1 hour | `server.servlet.session.timeout=1h` |
| 2 hours | `server.servlet.session.timeout=2h` |
| 8 hours | `server.servlet.session.timeout=8h` |
Step 4: Save Changes
Save the `application.properties` file after making your modifications.
Step 5: Restart the Service
For the configuration changes to take effect, restart the PowerChute Network Advanced Windows service:
- Open the Windows Services Manager (Start → Services, or run `services.msc`)
- Locate PowerChute Network Advanced in the list
- Right-click on the service and select Restart
- Wait for the service to fully restart. When the service has restarted, the PowerChute Network Advanced Configuration Tool can be accessed using a web browser as described in the user guide.
Notes
- Minimum Timeout: Must be greater than 0 (any positive value). Setting the value to `0` to configure sessions that never expire is not supported.
- Maximum Timeout: There is no upper limit for the timeout. However, very high values are not recommended for security reasons.
- Invalid values: If an invalid value is provided, the system will fall back to a default of 15m
- Default time unit A numeric value without a suffix is treated as milliseconds.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.