PowerChute Network Advanced - HTTPS Port Configuration
Issue
This article describes how to configure the HTTPS port for the PowerChute Network Advanced Configuration Tool. By default, the Configuration Tool operates on the standard HTTPS port 443. If this port is already in use on your system or if you prefer to use a different port, you can change it to an alternative port.
Products
PowerChute Network Advanced Configuration Tool version 1.0
Environment
Windows
Solution
Requirements
- Permission to edit configuration files in the PowerChute Network Advanced installation directory.
- Permission to restart Windows services.
- The desired port must be available and not in use by another service.
Configuration Steps
Step 1: Locate the Configuration File
Navigate to the config folder in your PowerChute Network Advanced installation directory and open the application.properties file in a text editor.
Step 2: Find the Server Port Property
Locate the following line in the configuration file:
# Server HTTPS port
server.port=443
Step 3: Modify the Port Value
Change the port value to your desired port number.
Step 4: Save Changes
Save the application.properties file after making your modifications.
Step 5: Restart the Service
For the configuration changes to take effect, restart the PowerChute Network Advanced Windows service:
- Open the Windows Services manager (Start → Services, or run services.msc).
- Locate PowerChute Network Advanced in the list.
- Right-click on the service and select Restart.
- Wait for the service to fully restart. When the service has restarted, the PowerChute Network Advanced Configuration Tool can be accessed using a web browser.
Step 6: Update Browser URL
When using a non-default HTTPS port, the port number must be included in the URL when accessing the Configuration Tool Web UI. Use the following format: https://<hostname>:<port>/
Examples:
Port Number Browser URL
Port 443 (default) https://localhost/
Port 8443 https://localhost:8443/
Step 7: Update Shortcuts (Optional)
You may want to update Start Menu or Desktop shortcuts that launch the PowerChute Configuration Tool. This can be done by updating the shortcut target to include the new port number in the URL.
The Start Menu shortcut can be found under "C:\ProgramData\Microsoft\Windows\Start Menu\Programs\PowerChute Network Advanced\". The shortcut is named "PowerChute Network Advanced".
The Desktop shortcut can be found under "C:\Users\Public\Public Desktop\". The shortcut is named "PowerChute Network Advanced".
Notes
- Port Availability: Check the port you select is not in use by another service.
- Default Port: Port 443 is the standard HTTPS port and does not need to be specified in the web browser URL. All other ports must be explicitly included in the URL.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.