How can we help you today?

What is the cable length from the outside of the battery pack to the connector of BR24BPG?

Question:

What is the cable length from the outside of the battery pack to the connector of BR24BPG?

Product Line:

APC BR24BPG External battery pack

Environment:

All serial numbers

Cause:

The customer is asking for the length of the cable on the battery pack BR24BPG.

Answer:

The cable length from the outside of the battery pack to the connector is :approximately" 30cm / 12 inches.

Image showing the length of the charging cable of a BR24BPG

If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center