How can we help you today?

NBRK0250A Rack Access Becomes Inaccessible After Network Cable Removal from Appliance.

Issue:
NBRK0250A Rack Access Becomes Inaccessible After Network Cable Removal from Appliance.

Product Line:
NetBotz 250A

Environment:
Firmware versions v3.2.0.2, v3.3.0.1, v3.4.1.1, v3.4.2.6

Cause: It has been found that leaving the network disconnected from the NBRK0250A causes rack access card swipes to fail after 10 to 15 minutes.

Resolution:
This is being looked at by engineering to be addressed in the future.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center