How can we help you today?

What does Ib (Design Current) represent in EcoSet Design?

Ib (Design Current) represents the current flowing through the selected circuit under normal operating conditions. It is calculated based on the connected load and the network configuration defined within the project.

The Ib marker helps users to:

  • Verify circuit breaker sizing.
  • Validate cable sizing.
  • Check circuit loading conditions.
  • Ensure compliance with protection and design rules.

For a compliant electrical design, the following relationship should be satisfied:

Ib ≤ In ≤ Iz

Where:

  • Ib = Design Current
  • In = Circuit Breaker Rated Current
  • Iz = Cable Current-Carrying Capacity

Displaying the Ib marker on the curve allows users to quickly compare the operating current against the protection device and cable ratings, helping to confirm that the circuit is correctly designed and protected.

ib

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center