How can we help you today?

In EcoSet Design, what is the Current tab in the Curves and Selectivity window used for?

The Current tab in the Curves and Selectivity window allows users to display and analyze key operating and fault current values directly on the protection curve graph.

These current markers provide a visual reference that helps users understand how the electrical installation behaves under both normal operating conditions and fault conditions.

The displayed current values may include:

  • Ib – Design Current
  • IefMin – Minimum Earth Fault Current
  • Ik3Max – Maximum Three-Phase Short-Circuit Current

By displaying these markers on the graph, users can:

  • Assess protective device operation and tripping behavior.
  • Verify cable and equipment protection.
  • Evaluate protection coordination and selectivity.
  • Compare fault current levels against protection settings.
  • Identify potential protection or sizing issues.

The Current tab provides valuable insights into circuit performance and helps engineers validate that protective devices are correctly selected and coordinated for the installation.

current

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center