How can we help you today?

How to order non-standard key numbers for Harmony XB4 and XB5?

1. What you need to know

XB4 and XB5 key switches are supplied with standard lock n° 455 E. For any other lock, keep the standard head reference and add a suffix: 10 (458 A), 12 (421 E), 14 (520 E) or 20 (3131 A) for the four alternative standard locks; D or TEC10 for the three specific locks; K (4 tumblers) or C (5 tumblers) for custom locks. In the custom case the radical alone is not enough - the key number must be entered as technical text on the order line, followed by the profile letter. Spare keys are ordered separately, using the radical ZBG followed by the key number.

2. What to check before ordering

A key number is not ordered like a product reference. It is built in two parts: a suffix on the head reference and, for custom locks, a technical text on the order line.

  • Wafers are the teeth of the key. 4 tumblers keys come in profile A or E, 5-tumblers keys in profile C.
  • A key carries two equivalent codes: a short indirect code (e.g. 422) and a direct code derived from the tumblers (e.g. A1323). Either is accepted on an order.
  • The number entered on the order is the one physically engraved on the key - a typing error ends up on the delivered product.
  • Suffix and technical text are not interchangeable: the suffix identifies the order radical, the technical text identifies the exact key. A K or C order without technical text cannot be produced.

3. Available locks and ordering rule

FamilyLock n°Suffix to addTechnical text requiredCompatibility
Standard (fitted as supplied)455 Enone-All XB4 and XB5 key switches
Alternative standard458 A10-All XB4 and XB5 key switches
Alternative standard421 E12-All XB4 and XB5 key switches
Alternative standard520 E14-All XB4 and XB5 key switches
Alternative standard3131 A20-All XB4 and XB5 key switches
Specific4A185D-Key-release emergency stop, body ZB5AS944
SpecificTEC10TEC10-XB4 key switches only, body ZB4BGxx
Specific8D1D-XB5 key switches only, body ZB5AGxx
Custom, 4 tumblersprofile A or EK4-digit number + profile letter (e.g. N° 1242 A)Any head whose standard reference is in key 455
Custom, 5 tumblersprofile CC5-digit number + letter C (e.g. N° 32432 C)Any head whose standard reference is in key 455

4. Schneider Electric references

FunctionReferenceProduct description
Key switch head XB5, 2 positionsZB5AG2Ø22 key switch head, plastic bezel, standard lock n° 455 E. This is the base reference to suffix.
Key switch head XB4, 2 positionsZB4BG2Metal equivalent of the ZB5AG2. Base for the TEC10, K and C suffixes.
Head with alternative standard lockZB5AG210Example of a suffixed reference: same head, lock n° 458 A. Same logic for 12, 14 and 20.
Emergency stop body, key releaseZB5AS944Key-release emergency stop. Suffix D for the 4A185 profile lock: ZB5AS944D.
Custom radical, 4 tumblersZB4BG2K / ZB5AG2KOrder radical. Cannot be produced without the technical text giving the key number and profile.
Custom radical, 5 tumblersZB4BG2C / ZB5AG2COrder radical for 5 tumblers, profile C. Same rule on the technical text.
Set of 2 keys, standard lockZBG455Set of 2 keys n° 455. Built as ZBG + key number: ZBG421E, ZBG458A, ZBG520E, ZBG3131A.
Set of 2 keys, 8D1 lockZBD8D1Key set for the 8D1 profile lock used on XB5 key switches.
Custom key setZBGK / ZBGCZBGK for 4 wafers (profile A or E), ZBGC for 5 tumblers. Technical text: the direct or indirect code of the lock.

Contact Schneider Electric Technical Support to check key lock feasibility before ordering.

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center