Compact to X80 quick wiring adapter - 990XSM00206
Issue
Migrating the following Compact IO cards to their X80 equivalent and need to confirm the 990XSM00206 quick wiring cable pinout.
AS-BDEP-214 -----> BMXDDI1602/1603
AS-BDEP-216 -----> BMXDDI1602
AS-BDEP-254 -----> BMXDDI1602H/1603H
AS-BDEP-256 -----> BMXDDI1602H
AS-BDEP-257 -----> BMXDDI1604T
AS-BDEP-297 -----> BMXDDI1603
AS-BDEO-216 -----> BMXDDI1602
AS-BDAO-216 -----> BMXDDO1602
AS-BDAP-208 -----> BMXDRA0815
AS-BDAP-258 -----> BMXDRA0815H
AS-BDAP-216 -----> BMXDDO1602
AS-BDAP-256 -----> BMXDDO1602H
AS-BDAP-217 -----> BMXDRA0815H
Product line
Modicon X80, M340, M580
Resolution
Below is an image of the pinout.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.