How can we help you today?

What is the wiring method for XB4BD912R* and XB5AD912R* potentiometers?

1. What you need to know

The Harmony XB4BD912R* (metal) and XB5AD912R* (plastic) potentiometers have three terminals: A and C are the two ends of the resistive track, B is the wiper. Wire all three for a voltage divider, typically to supply a speed reference to a variable speed drive. Wire the wiper plus one end only for a variable resistor. The terminals are marked on the potentiometer body.

2. Understanding the three terminals

Both ranges share the same electrical layout — only the bezel material differs. The wiring depends on the function you need, not on the range.

  • Terminals A and C carry the full resistance value; terminal B is the wiper, whose resistance varies with knob position.

Understanding the three terminals of Harmony potentiometers

  • A potentiometer has no polarity: swapping terminals A and C reverses the direction of adjustment but causes no damage.
  • Rating is 1 W, linear law, with values from 1 kΩ to 470 kΩ.

3. Voltage divider and variable resistor

CriterionVoltage dividerVariable resistor (rheostat)
Wiring exampleHarmony potentiometer wiring example - Voltage dividerHarmony potentiometer wiring example - Rheostat
Output deliveredA voltage proportional to knob positionA resistance varying with knob position
Typical applicationSpeed reference on VFD analog inputResistive setpoint, lamp dimming
Typical value10 kΩ for a 0…10 V drive inputMatched to circuit impedance
Supply neededYes, across terminals A and CNo

4. Schneider Electric references

FunctionReferenceDescription
Complete potentiometer, metalXB4BD912R10KHarmony XB4, Ø22, 10 kΩ, 1 W, linear — most common value for drive control
Complete potentiometer, metalXB4BD912R1KHarmony XB4, Ø22, 1 kΩ, 1 W, linear
Complete potentiometer, plasticXB5AD912R10KHarmony XB5, Ø22, 10 kΩ, 1 W, linear
Complete potentiometer, plasticXB5AD912R1KHarmony XB5, Ø22, 1 kΩ, 1 W, linear

Launch Product Selector on se.com to configure a Harmony potentiometer according to your requirements or contact Schneider Electric Technical Support to check a configuration against your control scheme.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: