How can we help you today?

PowerChute is flagged a vulnerable to CVE-2026-49844

Issue:

PowerChute is flagged a vulnerable to CVE-2026-49844

Product:

PowerChute Serial Shutdown 1.5, 1.6

PowerChute Network Shutdown 5.2

Environment:

All supported operating systems.

Cause:

PowerChute Serial Shutdown 1.5 and 1.6 ship with Log4j versions less than version 2.25.5

PowerChute Network Shutdown 5.2 ships with Log4j versions less than version 2.25.5

Solution:

For PowerChute Serial Shutdown 1.5, 1.6 on Windows:

  1. Download the attached file PCSS_Log4j_Update.zip file
  2. Uncompress the file PCSS_Log4j_Update.zip
  3. Open a command prompt as an administrator
  4. Change directory to the PCSS_Log4j_Update.zip directory that was created when the zip file PCSS_Log4j_Update.zip was uncompressed.
  5. Run the command run_patch.cmd

The patch will remove the current log4j files and replace them with log4j version 2.26.1.

For PowerChute Network Shutdown 5.2 on Windows:

  1. Download the attached file PCNS5.2_log4j_update.zip file
  2. Uncompress the file PCNS5.2_log4j_update.zip
  3. Open a command prompt as an administrator
  4. Change directory to the PCSS5.2_log4j_update directory that was created when the zip file PCSS5.2_log4j_update.zip was uncompressed.
  5. Run the command run_patch.cmd

The patch will remove the current log4j files and replace them with log4j version 2.26.1.

For PowerChute Network Shutdown version 5.2 on Linux

  1. Download the attached log4j-2.26.1.tar file, and if needed, copy the file to the Linux system.
  2. Uncompress the log4j-2.26.1.tar file. The command is tar -xvf log4j-2.26.1.tar.
  3. Stop the PowerChute service. The command is systemctl stop PowerChute
  4. Change directory to the PowerChute lib directory. The default path is /opt/APC/PowerChute/group1/lib
  5. Move the log4j2 files to the APC directory. If PowerChute resides in the default path, the command is mv /opt/APC/PowerChute/group1/lib/log4j2* /opt/APC
  6. Change directory to the log4j-2.26.1 directory that was created when you uncompressed the tar file.
  7. Copy the log4j-api-2.26.1jar, log4j-core-2.26.1.jar, log4j-slf4j-impl-2.26.1.jar to the PowerChute lib directory that resides where PowerChute resides. If PowerChute resides in the default path, the command is cp log4j2* /opt/APC/PowerChute/group1/lib
  8. Start the PowerChute service. The command is systemctl start PowerChute

For PowerChute Serial Shutdown versions 1.5 and 1.6 on Linux

  1. Download the attached log4j-2.26.1.tar file, and if needed, copy the file to the Linux system.
  2. Uncompress the file. The command is tar -xvf log4j-2.26.1.tar.
  3. Stop the PowerChute service. The command is systemctl stop PBEAgent
  4. Change directory to where PowerChute has been installed. The default path is /opt/APC/PowerChuteSerialShutdown/Agent/
  5. Move the current log4j files. If PowerChute was installed to the default path, the command is mv /opt/APC/PowerChuteSerialShutdown/Agent/lib/log4j* /opt/APC
  6. Change directory to the log4j-2.26.1 directory that was created when log4-2.26.1.tar was uncompressed.
  7. Copy the new logj4 files to the PowerChute lib directory. If PowerChute was installed to the default path, the command is cp log4j.* /opt/APC/PowerChuteSerialShutdown/Agent/lib
  8. Restart the PowerChute service. The command is systemctl start PBEAgent

Schneider Electric Egypt and North East Africa

Attachment(s)
Log4j-2.26.1.tar [2.29 MB]
PCSS_Log4j_Update.zip [2.02 MB]
PCNS5.2_log4j_update.zip [2.02 MB]
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
  • Help and Contact Center