How can we help you today?

Why my BMENUA0100 is not NTP synchronized in “CA only” or “Selfsign & CA” mode?

With BMENUA0100 FW 3.01.34, it is important to synchronize the module with an NTP server before changing the PKI mode.

After a Factory Reset, the BMENUA0100 starts in “Self-Signed only” mode.

1

Before switching to “CA only” or “Selfsign & CA”:

  • Check that the NTP Client Service to “ON”.
  • Wait until the BMENUA0100 is correctly synchronized.
  • Check that the date and time displayed on the Home page are correct.

1

  • Change the PKI mode to “CA only” or “Selfsign & CA”.

3

The BMENUA0100 will then restart with the NTP Client Service set to “OFF”, while retaining the correct date and time.

4

An incorrect module time may cause problems when importing a CA-signed certificate.

Once the CA-signed certificate is imported and new configuration applied to the BMENUA0100 module, the NTP client Service will be set to "ON"

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center