How can we help you today?

What is the default IP address of the M172 Secure Interface Gateway when connected via USB?

Issue:

Default IP address of the M172 Secure Interface Gateway when connected via USB


Product Line:

M72


Resolution:

The default IP address after the connection of a PC to TM172 Secure Interface Gateway via USB mini-B connector is 192.168.254.254 .

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center