How can we help you today?

EAE26.0 : How to open weblinks from EAE Windows HMI

This knowledge base article explains users on how to open weblinks from Ecostrusure Automation Expert HMI.

  1. Take a Button on to the HMI Canvas and name it as WebLink as shown below.

w1

2. Double Click on the added button to open C# source code and Once C# code opened, make sure “System.Diagnostics” library is referenced if not then add it manually as shown below.  .

w2

3. Locate the button name as shown below .

w3

4. Under that, kindly write the function, Process.Start("URL"); command for added button to open URL as shown below. In this example we are opening the weblink "https://www.se.com/in/en/product-range/23643079-ecostruxure-automation-expert/"

w4

5. Build and then RUN the HMI. Upon clicking the button the website will be opened. Kindly note that this will work with only Windows HMI Projects.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center