How can we help you today?

How many open connections the OPCUA Server of BMEECN0100 opened to the M580 Controller ?

The OPC UA Server of the BMEECN0100 opens the following number of connections depending of the M580 controller model and his capacity.

Thus, performance of the BMEECN0100 module depends on the time required to perform the MAST task and the selected controller.

The maximum number of connections opened by each BMEECN0100 module to the M580 controller are as follows:

1

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center