How can we help you today?

What baud rates are supported by the EM4200 Series Power Meter?

Issue

Customer is looking for device communication specifications and needs to know the baud rates that are supported by the device.

Product Line

EM4200 Series Enercept Power and Energy Meters

Environment

Hardware & Hardware Communications (Modbus, BACnet, etc.)

Cause

The supported serial communication rates and automatic communication detection capabilities need clarification.

Resolution

Communicating models of the EM4200 Series automatically detect the baud rate, parity, and communication protocol.
The meter supports Modbus RTU and BACnet MS/TP communication at serial rates up to 115.2 kbaud, equivalent to 115,200 baud.

Additionally, The EM4200 also automatically detects and selects the appropriate communication protocol and parity settings.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center