{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

How to calculate earth fault loop impedance value (Zs) ?

the Breaker Earth Loop Impedance (Zs) is calculated as follows; Zs = Uo / Ia Where Uo is the voltage to earth and Ia is the current to trip the breaker in a given breaker disconnection time. Usually...

What is the download link for the trial version of Unity Pro XL 8.0 ?

Please check the link below to download Unity Pro S/L/XL V8.0 trial version , taking into consideration that the Unity Pro trial software will run for 21 days before it expires....

What is the difference between type A & AC class RCCB ?

In Class A (Tripping is ensured for sinusoidal, alternating residual currents as well as for pulsed ,DC residual currents, whether they are quickly applied or slowly increased. Application: loads...

What is the definition of ANSI 50N/51N or 50G/51G - Earth fault?

Earth fault protection based on measured or calculated residual current values: ANSI 50N/51N: residual current calculated or measured by 3 phase current sensors ANSI 50G/51G: residual current...

Please send me the X/R ratio of transformer for 1600kVA Trihal transformer?

The X/R ratio for the 1600kVA Trihal transformer can be calculated using the Trihal electrical characteristics (impedance & losses data) given normally in transformer datasheets (attached )...

What is the service breaking capacity and what is the advantage of that on...

In a correctly designed installation, a circuit-breaker is never required to operate at its maximum breaking current (Icu). For this reason, a new characteristic has been introduced which is the...

What is a 1 or a 2 gang light switch?

"Gang" describes the number of switches on the plate. They are sometimes called rockers, throws or dimmers, depending on how they operate, but still they just refer to the number of light...

What is meant by vector group for transformers and why is it important?

What is vector group for transformers? A vector group is the International Electrotechnical Commission (IEC) method of categorizing the high voltage (HV) windings and low voltage (LV) winding...

Show more

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
Show more

Learn more through our Generic Knowledge FAQsGeneral Knowledge

What is meant by Symmetrical and Asymmetrical breaking currents?

issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...

In a 3 phase system, why does the meter still show voltage reading on one...

Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...

What is the selection criterion of Circuit Breakers for the Capacitor bank...

The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase nominal current up to 1.5In. The Derating...

How to reset Zelio logic password?

The password can be reset by clearing the program inside the Zelio either by Transfering a new program to the Zelio Or Clearing the program that already exist by updating the firmware Kindly find the...