- PT100 is an RTD (Resistance Temperature Probe) made of Platinum metal which has a resistance value of 100 ohms at zero degrees celsius. - PTC (Positive Temperature Coefficient) and NTC (Negative...
Rated impulse withstand voltage (Uimp): The peak value of an impulse voltage of prescribed form and polarity which the equipment is capable of withstanding without failure under specified conditions...
Earth fault protection based on measured or calculated residual current values: ANSI 50N/51N: residual current calculated or measured by 3 phase current sensors ANSI 50G/51G: residual current...
The difference is indicated below : Closing release XF : The XF release remotely closes the circuit breaker if the spring mechanism is charged. Opening release MX: The MX release instantaneously...
International standard EN/ISO 13850 (replaces standard EN 418) specifies the functional requirements and design principles of emergency stop devices. Stop types: Stop category 0 and/or stop category...
In a correctly designed installation, a circuit-breaker is never required to operate at its maximum breaking current (Icu). For this reason, a new characteristic has been introduced which is the...
the Breaker Earth Loop Impedance (Zs) is calculated as follows; Zs = Uo / Ia Where Uo is the voltage to earth and Ia is the current to trip the breaker in a given breaker disconnection time. Usually...
Issue You wish to upgrade your Network Management Card's (NMC) firmware or have been instructed to. You have a device such as a Smart-UPS, Smart-UPS Ultra, Easy UPS On-Line, Easy UPS 3-Phase,...
issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...
There is often confusion between the in-phase and the In-sync features of ASCO transfer switches. It is important to understand the difference between these features especially during the process of...
Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...
Issue: Having two different values for RL ( Lead resistance from the CT to the relay); RL from the phase CT to the relay and RL from the neutral point CT to the relay Environment: Protection Function...
The password can be reset by clearing the program inside the Zelio either by Transfering a new program to the Zelio Or Clearing the program that already exist by updating the firmware Kindly find the...
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.