Roll over image to zoom in

SP-C-IP
Access control solution with large user capacity and extensive features
Extending the Security Expert system with on board local inputs and outputs
Allows cost effective expansion without the increased cost of modules
RS-485 communication interface, 2400 bps modem and an Ethernet port
A complete solution for system expansion, offsite monitoring
Environmental Data
Use Better
Packaging made with recycled cardboard
No
Use Again
Take-back
No
Need more information? Check our technical FAQs!
Easily find answers to the most frequently asked questions.