Why are microgrids important?
Microgrids are important because they give organisations a local, controllable source of power that can keep operating when the main grid fails. They improve energy efficiency, resilience, decarbonisation, and access to energy by combining on-site renewables, batteries, and smart controls. They also help cut costs by storing power, reducing peak-demand charges, and exporting excess electricity back to the grid.

A microgrid is a localised energy system that can generate, store, and manage electricity independently or alongside the traditional utility grid. A microgrid generates, stores, and manages power right where it is consumed. Unlike the main utility grid, a microgrid can operate in two modes: Grid-connected, where it exchanges power with the utility network, and islanded, where it disconnects and runs independently during outages or disturbances.
The "island mode" is the main difference between the two - during a utility outage the microgrid can disconnect from the main grid and continue supplying power locally, making it highly valuable for resilience and business continuity. The utility grid is centrally operated and designed for large-scale power delivery, whilst a microgrid uses local intelligence to balance supply and demand in real time, prioritising critical loads. Microgrids also support sustainability goals by integrating renewable energy, reducing carbon emissions, optimising energy efficiency, and lowering peak demand charges. Get answers to the ten key questions on why and how microgrids are essential.
A microgrid requires a combination of energy resources, control systems, and electrical infrastructure that work together as one coordinated system.
Energy and storage
At the core are distributed energy resources such as solar, wind, fuel cells, or backup generators, which provide local power generation. Energy storage systems—mainly lithium-ion batteries—are essential to absorb excess energy and respond quickly to disturbances.A microgrid makes financial sense when the combined value of resilience, electricity grid disruptions, energy savings, sustainability, and flexibility outweighs the capital and operational cost of the system. The strongest business cases are usually in locations with high outage costs, expensive, volatile electricity prices, or strong incentives for distributed energy. These are industries such as data centres, manufacturing, hospitals, industrial plants, universities, where even short outages can lead to significant financial, safety, or reputational losses. Microgrids are becoming more economically attractive by reducing peak demand charges, optimising energy use, integrating renewable energy, and shifting energy use with batteries when grid power is most expensive. Financial viability also improves when projects can leverage government incentives, tax credits, carbon reduction incentives, or avoided infrastructure upgrades. Learn more about the economic benefits of microgrid adoption in a Schneider Electric blog post.
Yes, a microgrid can run on 100% renewable energy, but whether it can do so reliably and cost-effectively depends on design, energy demand, load profile, intelligent management, and local conditions. Most renewable microgrids combine wind, solar, hydro, or biomass generation with battery energy storage systems and advanced automation controls to balance supply and demand in real time. Intermittency is the main challenge - solar and wind output fluctuate daily and seasonally, so a 100% renewable microgrid must be sized with sufficient storage duration and generation diversity to maintain power during low-generation periods. In practice, organisations aim for a 100% renewable operation, rather than complete energy independence, using hybrid systems that include backup generation and long-duration storage. Even so, renewable microgrids can significantly reduce carbon emissions, fuel consumption, and operating costs whilst improving resilience. If you are looking for more information on combining renewable energy with microgrids read our articles on adding a microgrid to a solar energy system or the impacts of battery storage on microgrids.
Islanding is the ability of a microgrid to disconnect from the main utility grid automatically and operate independently, during power outages, grid instability, or emergency. When this happens, the microgrid controller detects abnormal conditions and initiates a controlled separation (within milliseconds) using protective relays and breakers. After the separation, the microgrid's controller immediately rebalances local generation (like solar or wind) and energy storage (batteries) to match the facility's real-time electricity demand. Finally, the main grid is restored, the microgrid synchronises its voltage and frequency before reconnecting safely. Islanding is safe when designed according to modern electrical standards and is managed by an intentional microgrid system. Modern microgrids follow strict interconnection standards, and protection schemes to prevent unintentional backfeeding, which could endanger utility workers. Continuous monitoring, fail-safe controls, and regular testing ensure that islanding occurs only under appropriate conditions.
Artificial intelligence transforms microgrids from rule-based systems into adaptive self-optimising energy platforms. Traditional microgrids rely on predefined logic and static schedules, whilst AI algorithms analyse massive datasets—including hyper-local weather feeds, historical usage patterns, and real-time electricity pricing to make real time decisions. This allows the microgrid controller to proactively dispatch solar, batteries, and generators, reducing costs and improving reliability. Smart algorithms also detect equipment faults, cyber threats, and abnormal energy patterns in real time, helping operators prevent outages before they occur and extend asset life. Moreover, predicting utility price spikes, the AI autonomously executes arbitrage, charging batteries when grid power is cheapest and discharges them to the facility when process goes up, maximising ROI. Download our report on AI-Powered Microgrids to uncover the full potential of AI and microgrids.
A microgrid is typically built by a coordinated group of players rather than a single company. The site owner—such as a corporation, campus, hospital, or municipality—sets the goals for cost, resilience, or carbon reduction. A microgrid developer or integrator then leads the overall project, supported by EPC firms that physically design and construct the system. Technology providers supply the core assets like solar, batteries, generators, and control software, whilst utilities approve interconnection and define operating rules. Financing partners and energy service companies often structure and fund the project, and software and control providers (such as Schneider Electric) optimise how all the assets operate together in real time.
The microgrid market is commonly described in industry analyses such as Guidehouse reports as being led by global integrated energy and automation companies like Schneider Electric, Siemens, Hitachi Energy, GE Vernova, and ABB. These leaders compete alongside utility-affiliated developers such as Engie, Enel X, and EDF Renewables, as well as specialised microgrid firms like Wärtsilä, PowerSecure, Scale Microgrid Solutions, and Bloom Energy. Across the market, Guidehouse consistently highlights a shift towards fully integrated providers that combine hardware, software, EPC capabilities, and financing under one coordinated solution.
A microgrid can save money, but the outcome depends heavily on-site conditions and energy usage. Savings typically come from reducing peak demand charges, shifting energy use to lower-cost periods, and avoiding expensive outages or downtime. Sites with high electricity costs, volatile tariffs, or critical operations that already require backup power tend to see the strongest financial benefit. However, microgrids are best understood not just as a cost-reduction tool, but as a combined strategy for cost optimisation, resilience, and energy control.
A microgrid can also significantly reduce carbon emissions when it is designed to integrate renewable energy like solar and supported by battery storage. By displacing grid electricity and reducing reliance on fossil-fuel backup generators, it lowers overall emissions. Storage further improves impact by enabling renewable energy use when it is needed rather than when it is produced. The overall carbon benefit depends on how clean the local grid is and how the system is operated, but in most cases a well-designed microgrid materially reduces a site's carbon footprint whilst improving energy reliability.
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.