Search FAQs
Rope pull switches XY2C - Is it possible to replace the XY2CE reset button ZB5AP6S by a standard Harmony reset like the ZB5AA2?
This is not allowed because the reset button of the XY2CE rope pull switch, is a special one with a travel different from the standard Harmony reset like the ZB5AA2 one for example. Attached Preventa XY2C catalogue extract with the following reset references in spare parts. Please select the dedicated reset button, not the standard one. Alone impact on the reset function of the switch (inoperative), not on the tripping (safety function). Please note that this reset button (ZB5AP6S) has been assembled in the XY2CE front cover in stainless steel from 3Q2012, with the red color of the casing
Released for:Schneider Electric Indonesia
Attachment(s)
Explore more
Explore more