Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
3 Easy Ways to Choose the Right Contactor

There are three way to selection of contactor:

1. Types of applications, there are many application characteristics (utilization categories): such as AC-1, AC-3, AC-4 and other categories.
https://en.wikipedia.org/wiki/Utilization_categories

2. The size of the rating specification: load power, operational voltage and coil voltage.

3. number of poles (normally open and normally closed contact) and also auxiliary contact.

Schneider Electric Indonesia
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
  • Legal information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings