FAQ Pencarian
ION Enterprise 6.0 SP1 Installation Procedures for New Systems (Includes Windows 7 and Server 2008 32-bit and 64-bit)
To provide step by step instructions for installation of ION Enterprise 6.0 SP1.
Product Line
ION Enterprise 6.0 SP1
Environment
Installation
Cause
To provide platform dependent step-by-step instructions for the installation of ION Enterprise 6.0 SP1 with a focus on installing ION Enterprise on the newer operating systems - Windows 7 and Windows Server 2008 R2.
ION Enterprise 6.0 was released before these new operating systems were available so it is important to follow the instructions we are providing to ensure a successful install, particularly for the Web Reporter component.
Resolution
This document contains instructions for deploying ION Enterprise 6.0 SP1 on both standalone and distributed configurations. Be aware that for distributed configurations firewall considerations are not addressed.
Caution: This article contains advanced configuration instructions and should only be implemented by experienced Application Engineers (Engineering Services) and ION Enterprise administrators.
Other relevant articles to read:
FA212496 - RS2008WRConfigurationWizard
Choose from the support matrix of ION Enterprise deployment scenarios based on the following criteria.
1. Network Topology Supported topologies include Standalone Primary Server or Database Server + Application Server.2. Operating System
3. SQL Server Version
Causes and Fixes
Supported Standalone ION Enterprise Deployments1 - IONE6_Win7_32bit_SQL2005_Express_32bit
2 - IONE6_Win7_32bit_SQL2005_Standard_32bit
3 - IONE6_Win7_32bit_SQL2008_R2_Standard_32bit
4 - IONE6_Win7_64bit_SQL2005_Express_32bit
5 - IONE6_Win7_64bit_SQL2005_Standard_64bit
6 - IONE6_Win7_64bit_SQL2008_R2_Standard_64bit
7 - IONE6_Win2008_32bit_SQL2008R2_Standard_32bit_Standalone
8 - IONE6_Win2008R2_SQL2005_Express_32bit_Standalone
9 - IONE6_Win2008R2_SQL2005_Standard_64bit_Standalone
10 - IONE6_Win2008R2_SQL2008R2_Standard_64bit_Standalone
Supported Database Server + Application Server ION Enterprise Deployments
11 - IONE6_Win2008_32bit_SQL2008R2_Standard_32bit_Distributed_DB
12 - IONE6_Win2008R2_SQL2005_Standard_64bit_Distributed_DB
13 - IONE6_Win2008R2_SQL2008R2_Standard_64bit_Distributed_DB
14 - IONE6_Win2008R2_SQL2008R2_Standard_64bit_Minimalist_DB
Download the appropriate instructional document for your deployment scenario.