Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why can't I find combination Motor Starters (e.g. GV2DM202) on the My Schneider site?

In the UK we do not offer pre-assembled combination starters, but we do offer the individual parts to make them up. The assembly is a very short and simple process.

Each starter is made up of  a GV2 manual motor starter and a contactor (LC1D or LC1K) plus an adaptor to join the two together. The section of the catalogue for combination starters lists the part numbers of the individual parts required.

Example
D.O.L Reversing starter GV2DM202**

This is made from the following:

  • Motor Circuit Breaker GV2ME02
  • Contactor LC2D09**
  • Combination Block GV2AF3


Note
** refers to the coil voltage code eg BD for 24Vdc

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre