Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I have remote operation with RM6 RMU?

Remote operation can be enabled by integrating a RTU (Remote Telecontrol Unit) such as PowerLogic™ T300 and fitting actuators to the required functions. It may also be necessary to add additional wiring to enable the RTU to be integrated and commissioned prior to putting it back into service.

For more information on:  -

Schneider Electric Ireland