Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What size cables can be terminated into NSX100-250 MCCBs?
Compact NSX MCCB types NSX250, NSX160 & NSX100 accept cables up to 95mm2 using crimp lugs.

The lug sizes are:
NSX100 is M6
NSX160 and NSX250 is M8

If terminating 120, 150 or 185mm cables then cable spreaders and/or the reduced crimp lugs should be used. This is based on a single core Cu cables.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre