Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the distance between centers of the 400A & 630A outgoing SAIF fuseways?
Standard 400 & 630A rated SAIF fuseways mounted on the busbars inside feeder pillars and fuse cabinets with a pitch of 120mm between centres.
This distance will increase if large or multiple cables are to be terminated, i.e. more than 1 x 4 core 300mm.

Schneider Electric Ireland
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
  • Help and Contact Centre