Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the distance between centers of the 800A outgoing SAIF fuseways?

Standard 800A rated SAIF fuseways mounted on the busbars inside feeder pillars and fuse cabinets with a pitch of 160mm between centers.
This distance may increase if large or multiple cables are to be terminated, i.e. more than 1 x 4 core 300mm or single core 630mm cables.

For more details, you can refer to page 27 of the catalogue.

Schneider Electric Ireland

Attachment(s)
SAIF Brochure Web.pdf [2.43 MB]