Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What replaced the XPSAX safety relays? What are the differences between XPSAX and the XPSAC?
NOTE - The XPSAX range was initially replaced by XPSAC, which has itself now been replaced by XPSBAC. You'll find a document attached to this FAQ detailing the changes from XPSAC to XPSBAC.  If you are replacing the XPSAX with the latest XPSBAC, you will need to follow the changes from XPSAX to XPSAC, then to XPSBAC to ensure your wiring is correct.
XPSAX                                                                                      XPSAC


XPSAX XPSAC

The main differences are as follows:

  • XPSAC has a solid state output for PLC signaling
  • XPSAX has one additional N/C output
  • XPSAC has larger range of supply voltage selection
  • XPSAC has choice between 2 models with or without removable plug terminals (Add 'P' to the end of the part number)

    Schematic Comparisons
    Monitoring of E-stop with 2N/C contacts


Monitoring of Estop with 2NC contacts

Monitoring of E-stop with 1N/C contact



Monitoring of Estop with 1NC contact

Cross Reference Table

XPSAX to XPSAC

Schneider Electric Ireland

Attachment(s)
XPSAC-XPSAXE-XPSBAC.pdf [537.25 KB]
Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre