Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which Schneider Electric Drive has replaced the Telemecanique Altivar ATV68?

The ATV68 is currently replaced by the the ATV600 and ATV900 series drives, for completeness below are the details for replacement of an ATV68 with an ATV61/71.

For ATV68 to ATV 600 or ATV900

The ATV61/71, drives, now superseded by the ATV600 and 900 series, and the way that these drives are selected is different to the previous ranges of drives as they are now a called a process drive. On the process drive you need to select the drive based on the  application that the drive is to be applied to, pumps /fans or a machine tool / hoisting drive, and then the power rating from either the standard or heavy duty modes of the drive. Therefore it is difficult to do a direct comparison from the old range to the new range of drives.

( Please see below the list of the closest alternatives based on the overcurrent ratings and the application type the drives are to be used for).


For ATV68 to ATV61/71

There are two possible replacements as the ATV68 could be used on High Torque applications or on Standard Torque applications so listed below are the possible replacements

Three Phase Supply 400.....500V 50/60H

High Torque Applications (150% Tn)  Machines and hoisting applications

ATV68C10N4 ATV71HD75N4  ATV930D90N4 (set to HD mode).

ATV68C13N4 ATV71HD90N4  ATV930C11N4 (set to HD mode).

ATV68C15N4 ATV71HC11N4   ATV930C13N4 (set to HD mode).

ATV68C19N4 ATV71HC13N4   ATV930C16N4 (set to HD mode).

ATV68C23N4 ATV71HC16N4   ATV930C22N4 (set to HD mode).

ATV68C28N4 ATV71HC20N4   ATV930D25N4C (set to HD mode).

ATV68C33N4 ATV71HC25N4   ATV930C31N4C (set to HD mode).

ATV68C43N4 ATV71HC31N4  Now an APM build drive

ATV68C53N4 ATV71HC40N4  Now an APM build drive

ATV68C63N4 ATV71HC50N4  Now an APM build drive


ATV68FC10N4 ATV71HD75N4 With Encoder card  ATV930D90N4 (set to HD mode). + VW3A3420

ATV68FC13N4 ATV71HD90N4 With Encoder card  ATV930C11N4 (set to HD mode).  + VW3A3420

ATV68FC15N4 ATV71HC11N4 With Encoder card  ATV930C13N4 (set to HD mode).  + VW3A3420

ATV68FC19N4 ATV71HC13N4 With Encoder card  ATV930C16N4 (set to HD mode).  + VW3A3420

ATV68FC23N4 ATV71HC16N4 With Encoder card  ATV930C22N4 (set to HD mode)  + VW3A3420

ATV68FC28N4 ATV71HC20N4 With Encoder card   ATV930D25N4C (set to HD mode).  + VW3A3420

ATV68FC33N4 ATV71HC25N4 With Encoder card   ATV930C31N4C (set to HD mode).  + VW3A3420

ATV68FC43N4 ATV71HC31N4 With Encoder card  Now an APM build drive

ATV68FC53N4 ATV71HC40N4 With Encoder card  Now an APM build drive

ATV68FC63N4 ATV71HC50N4 With Encoder card  Now an APM build drive


Standard Torque Applications (120% Tn)  ( ATV600 series aimed pump and fan applications  ATV930 aimed at machine tools).

ATV68C10N4 ATV61HD90N4    ATV630D90N4   or   ATV930D90N4

ATV68C13N4 ATV61HC11N4    ATV630C11N4   or   ATV930C11N4

ATV68C15N4 ATV61HC13N4    ATV630C13N4  or   ATV930C13N4

ATV68C19N4 ATV61HC16N4    ATV630C16N4  or   ATV930C160N4

ATV68C23N4 ATV61HC20N4    ATV630C22N4  or   ATV930C22N4

ATV68C28N4 ATV61HC25N4   ATV630C25N4  or   ATV930D25N4

ATV68C33N4 ATV61HC31N4   ATV630C31N4  or   ATV930C31N4

ATV68C43N4 ATV61HC40N4   Now an APM build drive

ATV68C53N4 ATV61HC50N4   Now an APM build drive

ATV68C63N4 ATV61HC63N4   Now an APM build drive


ATV68FC10N4 ATV71HD75N4 With Encoder card  ATV930D90N4 + VW3A3420

ATV68FC13N4 ATV71HD90N4 With Encoder card  ATV930C11N4 + VW3A3420

ATV68FC15N4 ATV71HC11N4 With Encoder card  ATV930C13N4 + VW3A3420

ATV68FC19N4 ATV71HC13N4 With Encoder card  ATV930C16N4 + VW3A3420

ATV68FC23N4 ATV71HC16N4 With Encoder card  ATV930C22N4 + VW3A3420

ATV68FC28N4 ATV71HC20N4 With Encoder card  ATV930C25N4 + VW3A3420

ATV68FC33N4 ATV71HC25N4 With Encoder card  ATV930C31N4 + VW3A3420

ATV68FC43N4 ATV71HC31N4 With Encoder card  Now an APM build drive

ATV68FC53N4 ATV71HC40N4 With Encoder card  Now an APM build drive

ATV68FC63N4 ATV71HC50N4 With Encoder card  Now an APM build drive

Schneider Electric Ireland
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
  • Help and Contact Centre