Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I simulate an application on XBTH, XBTP or XBTE with XBTL1000 without PLC?

In order to simulate an application for a Magelis XBT-H , XBT-P or XBT-E using the XBTL1000 without being connected to a PLC we need:

1) Open the Configuration > Dialogue Table
2) Uncheck the "Use Dialogue Table"
3) Click on "OK"
4) Open the Simulation > Simulation Application
5) Enter address 0 when simulation asks you to.

It is now possible to display the page sequences without getting the error code "Cannot write table".

Note:

This platform is discontinued. Please get access to our digital catalog https://digicat.se.com/ or contact our support center for more information about migrations to a newer platform.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre