Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the diagram of the BMXFCCxx3 cable?
The cables BMXFCCxx3 designed for connecting 40-pin connectors to 2xHE10 come in 6 different lengths:
• 0.5 meters, 20 wires: BMX FCC 053
• 1 meter, 20 wires: BMX FCC 103
• 2 meters, 20 wires: BMX FCC 203
• 3 meters, 20 wires: BMX FCC 303
• 5 meters, 20 wires: BMX FCC 503
• 10 meters, 20 wires: BMX FCC 1003
image1
The diagram below shows the connection of BMX FCC ••3 cables:
image2
The maximum torque for tightening BMX FCC ••• cable connection screws is 0,5 N•m (0.37 lb-ft).

Schneider Electric Ireland