Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do you have an example of communication between one M221 and one HMISTU using Modbus serial?

An example showing the communication between M221 and HMISTU is attached in this FAQ.
It contains the SoMachine Basic and Vijeo Designer program.
In those programs there are examples of read bits and words from the PLC and write bits and words in the PLC.
Also there is an example of transfer of a preset value to one timer.



Note: The application was made for SoMachine Basic now the software is EcoStruxure Machine Expert Basic.

Schneider Electric Ireland

Attachment(s)
TM221_HMISTU.zip [58.72 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre