Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the cassette used to connect the circuit breakers to the Powerpact 4 panelboards be ordered separately?

No, the cassette is factory fitted only to the MGP... range and PP4.... range of circuit breakers. For example MGP1003X or PP42504X references.

If you require a circuit breaker that's not available in the standard MGP... or PP4 .... offer, for example with a different trip unit, you will need to order the cassette and breaker together along with a separate trip unit. (Please order frame-only PowerPact 4 MCCBs, which are supplied without trip units, and you can add the desired trip unit separately)

Schneider Electric Ireland