Yes, two sets of current sensors can be connected to a Sepam series 80.
Both traditional current sensors (current transformers CT In/5A or In/1A) and LPCT sensors can be connected.
Only Sepam series 80 using transformer earth leakage protection (Sepam T87, M88 and G88) do not allow the use of LPCT sensors.
Released for: Schneider Electric Ireland