Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the advantages of the new MET148-2 temperature module for Sepam?
The new MET148-2 module replaces the MET148.

It allows up to 8 temperature probes to be connected, for measurement and protection purposes. Available since May 2002, it offers the following features:
  • Replacement for the MET148 already available for Sepam series 20, 40, 60 and 80
  • Improved safety and reliability for temperature measurements
  • Use of two modules with Sepam series 40, 60 and 80 (NB: only one module for Sepam series 20):
    • to use this facility, set the address for each module (with the power off)

Schneider Electric Ireland