Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the the cycle time of the Sepam series 80?
The cycle time is the time taken by the Sepam series 80 to carry out all rapid functions. Within a fixed cycle time of 14 ms, the following functions are carried out: Self-tests; Protection functions; Update of logic inputs; Control logic; Equation editor; Update of logic outputs.
Some of the slow functions (measurements).

Schneider Electric Ireland