Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the life of an RM6 cubicle mechanism and what servicing is required?

The life of the RM6 cubicle is 30 years. The mechanism is guaranteed to 1000 operations. Under normal operating conditions, no maintenance is required during this period. Beyond that, regular checks should be made.

For more information please see online RM6 product page and refer to the document 'Instruction sheet' under documents tab.

Schneider Electric Ireland