Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to retrieve a fault recording (OPG) in SFT2841 from the Sepam Series 20, 40, 60, 80 relays?
Steps to retrieve fault recording in SFT2841:
(Note: Screen Caps may appear differently depending on Sepam series)

1. Verify communication between PC and Sepam. This indicator is located on the bottom left-hand side of SFT2841 window.

Communication

2. Click on "fault recording" located on the Menu bar.

Fault recording

3. Select the desired waveform based on the date/time and then click on the "retrieve" button.

Waveform

4. Select the save location and click "save"

Save location

5. SFT2841 will take some time to download the OPG (fault recording). After the download is complete, SFT2826 must be activated in order to view the waveform capture. Click on "SFT2826 activation" in order to activate this software and view the downloaded waveform capture.

SFT2826 activation

Schneider Electric Ireland