Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I find the full part number or coil voltage for a Tesys D Contactor?

For the Tesys D contactor coils, there are three formats; the AC control coil, the DC control coil, and Tesys Green Electronic coils (only available on certain models).

  • For the DC control coil and for the Green Electronic coils, the full part number - including the suffix - is on the front of the contactor e.g. LC1D09BD or LC1D25BNE
  • For the AC control coil the start of the part number is on the front, but the coil voltage suffix is in a window on the top face near the back (assuming the contactor is panel mounted). This is because the coil in the AC control contactors can be changed.


Below is a video showing the location of the part number on example DC and AC control voltage contactors.


NOTE: There are generations of Tesys D contactors with slightly different designs (colour, curved edges etc.). The principle of locating the coil voltage and constructing the part number is the same regardless of the generation.

Schneider Electric Ireland