Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
MET 148-2 8-Temperature Sensor Module Installation Sheet.

The MET 148-2 module can connect eight temperature sensors (RTDs) of the same type:

• Pt100, Ni100, or Ni120 type RTDs, according to parameter setting
• Three-wire temperature sensors

The temperature measurement provides for thermal overload and temperature monitoring.

Please see attachment.

Schneider Electric Ireland

Attachment(s)
MET148-2.pdf [215.13 KB]