Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
MSA141 Sepam Analog Output Module Installation Sheet.
The MSA141 module converts one of the Sepam™ measurements into an analog signal. Measurement selection is determined by parameter setting:

• 0-10 mA, 4-20 mA, or 0-20 mA analog signal according to parameter setting.

To scale the analog signal, set minimum and maximum values of the converted measurement.

Example—the setting used to set phase current (Ia) as a 0-10 mA analog output with a dynamic range of 0-300 A is: minimum value = 0 maximum value = 300 (3000 .. 0.1A = 300.0 A)
Any one of the CCA770 (2 ft or 0.6 m), CCA772 (6.6 ft or 2 m) or CCA774 (13.1 ft or 4 m) cables connects a single module for each Sepam base unit.

See attachment.

Schneider Electric Ireland

Attachment(s)
MSA141.pdf [117.36 KB]