Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you reset a Tesys T (LTMR devices) back to factory settings?

The first and essential step is to stop the system, it cannot be in Run for this process to work.

You must then press the blue reset button for 15 seconds, until the Alarm LED blinks. Then, release the button.

Reset is complete, and the Tesys T unit will now enter setup menu.

Below is a video that shows the full process including the change in LED's and the Operator HMI

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre