Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you control the start/stop and speed of an Altivar 630/930 Drive with the Local HMI using the Local remote button?

With the Altivar 630/930 drives there are several ways that you can control the Run/Stop or other Input commands and the Speed control.

When testing or setting up a Variable Frequency Drive it is sometimes useful to test the Motor Drive combination from the HMI (Human Machine Interface) on the front of the drive.

The Local / Remote button is not configured by default.

For the local remote button to be active you need to do the following:

Navigate to the complete settings menu > go to the command and reference menu > scroll down to the HMI command menu > you can select bumpless or stop function.
( bumpless means you can change from terminal control to HMI control without stopping the drive), where the stop selection means when you press the local remote button the drive stops and then you have to issue a new run command from the new control position.

Once this selection is made press enter to store the choice and then press escape back to the main screen.





Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre