Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Sepam Relay Series 20, 40, 60 and 80 use the same communication protocol as the (ANSI) Digital relay (DR)?
The Digital Realy (DR) (Sepam 1000 Americanized) communicates with a protocol called Power Logic (Sy-Max).
The Sepam 20, 40, 60 & 80 uses Mod-Bus RTU, an Industry standard protocol developed by Modicon. These two relays cannot communicate on the same daisy chain. A device such as EGX, ethernet gateway, can interface the two protocols for a common host.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre