Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the minimum overload setting on the TM-D thermal magnetic trip units for NS & NSX breakers?

Article available in these languages: Turkish

Only the three and four pole devices can be adjusted, single and double devices are fixed.

The NS100 - 250 TM-D thermal / magnetic trip units (including Merlin Gerin NS breakers) have an adjustment range of between 0.8 - 1 times the rating (In) of the trip unit.

The NSX100 - 250 TM-D thermal / magnetic trip units have an adjustment range of between 0.7 and 1 times the rating (In) of the trip unit.

For breakers with a current rating above 250 A, we use electronic trip units (Micrologic).

Schneider Electric Ireland