Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the iCT contactors suitable for switching DC power systems?
The iCT contactors are suitable for switching 250V AC (1 & 2 pole) and 400V AC (3 & 4 pole) Utilization Category AC7a and AC7b

They are not suitable for switching DC current.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre